Video: How can you program the ATV21 or ATV212 drive so that you can run the drive without the motor?

Article available in these languages: Tiếng Phần Lan

Issue:
Configuring ATV212 Drive to Run Without Motor Connected

Product Line:
Altivar ATV21 ATV212 S-Flex enclosed

Environment:
All

Cause:
Need to test the drive to see if there is a problem with it or a need to run the drive open circuit without the motor connected to it.

Resolution:
Programming
Find F- - - Enter
Scroll to Output Phase Loss F605= 0 (deactivate)
Set supply voltage correction F307 to 2 (supply voltage uncorrected).
Now you can disconnect your motor leads, and run the drive open circuit to test.


Be sure to return the parameters to their original value once testing has been completed.

Schneider Electric Việt Nam

Phần đính kèm

ATV212_Programming_manual_EN_S1A53838_01.pdfATV212_Programming_manual_EN_S1A53838_01.pdf [3.49 MB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: