What is the ATV312 Modbus register number for Speed reference in RPM?

Issue:
ATV312 Modbus register number for Speed reference

Product Line:
ATV312, Altivar 312

Environment:
All ATV312 drives

Cause:
Needs to send speed reference in RPM over Modbus

Resolution:
The modbus address is 8602 (1-1 rpm, if bit 9 of CMI =0).

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: