What is the max Modbus TCP client and server connection number for M258 Ethernet?
For the M258 & LMC058 controller, the Ethernet limitation connections are :

SoMachine Protocol  : Maximum connection number = 4 (1)
Modbus Server connection : Maximum connection = 8
Modbus Client : : Maximum connection = 8
Modbus Device : Maximum connection = 2
Ethernet IP  Device : Maximum connection = 16
FTP Server : Maximum connection = 4
Web Server : Maximum connection = 10

Theses resources are independent between them (no link limitation connections between them)

(1) The maximum number of SoMachine Protocol is 4.
These connections can be :
One connection for the HMI
One for the OPC Server
One for the SoMachine software
One for the Trace object (oscilloscope function)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: