Video: How do you remove the front main cover on the ATV61 and ATV71 drives?
Issue:
Remove the front main cover on the ATV61/71 drives.

Product Line:
Altivar ATV61 ATV71

Environment:
All

Cause:
Needs to know how to remove the front cover to replace it or to add an option card.

Resolution:
Push in the two front tabs at the top of the drive while pulling the top cover toward you.

Tools needed: Flathead screwdriver.

photo 2 photo 1

IFrame

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: