StruxureWare Power Monitoring Expert (PME) 7.2 Web Reporter stop working after upgrading to Google Chrome 40
Issue:
The latest release of Chrome from Google (version 40.0.2214.91 m) blocks all plug-ins by default

Product Line:
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x

Environment:
Chrome 40+
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.0
Power Monitoring Expert Software Web Applications

Cause:
The Web Applications in PME require a Silverlight plug-in which is blocked by default by this release of Chrome.

Resolution:
The following will be displayed when a user navigates to the PME Web Applications in this new version of Chrome:



To get the web page to load properly, you'll need to allow the Silverlight plug-in to run. To do so, you can click on the little "puzzle piece" with the red X on it that appears in the address bar. From there, you'll see an option to always allow plug-ins, as in the screenshot below:



To get the web page to load properly, the user need to allow the Silverlight plug-in to run. To do so, you can click on the little "puzzle piece" with the red X on it that appears in the address bar. From there, you'll see an option to always allow plug-ins, as in the screenshot below:



If you're still experiencing issues with Source and Measurement selector in the Reports tab after you're logged in, please follow the workaround provided in FA235076.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: