What is the cfm rating of the NetShelter CX with AR4703 installed?
Issue:
Customers want to know the cfm rating of NetShelter CX cabinets with the AR4703 fan booster installed.

Product Line:
NetShelter CX.

Environment:
All versions and serial ranges.

Cause:
Installing the AR4703 increases the cfm of the NetShelter CX cabinet.

Resolution:
18U  with 1x AR4703 - 260 CFM
24U  with 2x AR4703 - 330 CFM
38U  with 3x AR4703 - 340 CFM

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: