Is the NetShelter CX available in different colors?
Issue:
Customers need to know what colors the NetShelter CX are available in.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Customers may want the NetShelter CX in a color other than the standard Light Oak.

Resolution:
The NetShelter CX is also available in Black (RAL 9005), Dark Gray (RAL 7016) and White (RAL 9003).
Please see the attached document for information on the available colors and part numbers.
Please contact your APC by Schneider Electric Rep for price and availability.

Schneider Electric Việt Nam

Phần đính kèm
20150303 NetShelter CX Colour Options 220v IEC Rev1.pdf [236.59 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: