Activating Unity Dif registration using the Schneider Electric License Manager returns a server login web page.

Issue
Activating Unity Dif registration using the Schneider Electric License Manager returns a server login web page.

Product Line
Unity Dif

Environment
Windows 7 Professional, Unity Dif v8.0

Resolution
If you try to activate the license for Unity Dif using the Schneider Electric License Manager web portal, the following window could get returned:
image1

This occurs because the registry setting for the License Manager is pointing to the old IP address for the verification server.
To resolve the issue, the registry needs to be edited to remove the registry key settings.  This can be performed by running the
appropriate attached registry edit files.

Note:
Rename the file 'LMs4Prod.txt' to 'LMs4Prod.reg' and it is used for Windows 32 bit operating system.
Rename the file 'LMs4ProdOn64Bit.txt' to 'LMs4ProdOn64Bit.reg' and it is used for a Windows 64 bit operating system.

Schneider Electric Việt Nam

Phần đính kèm
LMs4ProdOn64Bit.txt [148 Bytes]
LMs4Prod.txt [136 Bytes]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: