What PM800 resets are available in ION Setup 3.0

Issue
ION setup 3.0 can only clear alarm logs for the PM800 series. The customer wants to remotely trigger meter resets without utilizing a modbus testing tool (register writes)

Product Line
PM800 series

Environment
ION SETUP 3.0 build 14220

Resolution
This article describes a workaround to enable meter resets directly from ION Setup 3.0. The Setup screen in ION Setup is customizable and many resets functionalities can be added as shown below:

Screenshot1
The setup menu could be modified for either the default PM800 series template or any particular template. Before you begin, make sure ION Setup 3.0 is not running:
  1. Navigate to C:\Program Files (x86)\Schneider Electric\ION Setup\tables\SQD800 and then select the default template you would like to modify
  2. Right click on Setup.cfg and uncheck the read only option
  3. Right click on Setup.cfg and edit using notepad
  4. Locate the [Meter Resets] section and modify it as shown in the text file attached
  5. Save the Setup.cfg file and then launch ION Setup 3.0
  6. Navigate to your device and make sure you choose the appropriate template options as shown below
Screenshot2

*Note: The latest version of ION Setup is currently ION Setup 3.2 and can be downloaded from here: ION Setup Latest Release | Schneider Electric. It is recommended to upgrade to the latest version of ION Setup.

Schneider Electric Việt Nam

Phần đính kèm

NewMeter_reset.txtNewMeter_reset.txt [642 Bytes]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: