What can cause an PTFL fault on the ATV61 and ATV71 drives?
Issue:
PTFL fault on the ATV61 and ATV71 drives.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Drive is faulting on power up.

Resolution:
This is a PTC error fault.   Check to see if the PTC switch is turned ON if so check to see if the PTC input is open or shorted.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: