How can you put the ATV61 and ATV71 drives in a NET command control mode?
Issue:
ATV61 and ATV71 drives controlled in a NET command control mode.

Product Line:
Altivar ATV61 and ATV71 with an Serial communications option card.

Environment:
All

Cause:
The drive is showing Terminal control mode they need to set it up for NET control.

Resolution:
Basic Programming settings will be
Set up your communications card in menu 1.9
In Menu 1.6:
-Set your Ref 1 1 channel to com card
-Set your Profile to be not separate
or
Set your Profile to be Separate  then CMD switching to a logic input or choose channel reference as com card.

Attached is the ATV61 Programming Manual to assist if needed.

Schneider Electric Việt Nam

Phần đính kèm
atv61_programming_manual_en_1760649_08.pdf [4.35 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: