Basic TCP/IP ports used by the WebDesigner tool…
The modules and Web Designer uses well known ports FTP (21), HTTP (80), SMTP (25), DNS (53) ,DHCP (67,68), NTP (123),SNMP (161,162) and Schneider application protocol (502). It also uses un-privileged ports (greater than 1024) for database access (depending on DB server configuration) and publish subscribe mechanism (6010 + dynamic port allocation). Then if you plan to use Web Designer through a firewall, you must check if all ports are opened for your module.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: