what are the OIDs for reading the LED status from Connexium Ethernet Switch TCSESM083F23F1 using SNMP Protocol in a MIB browser.
Issue:

Customer wants to read LED status on the ethernet switch using SNMP protocol.

Product Line:

Connexium Ethernet Switch TCSESM083F23F1

Environment:

Windows 7 Pro, iReasoning MIB browser

Resolution:

The very first step is to install the correct MIB file in the MIB Browser.
We need to install the two files in the MIB Browser.
1.SchneiderTFE-V03-00.mib
2.SchneiderElectricSwitches_V02_00.mib.
Contact your local country Schneider Electric Customer Care Center to get this files.

The LED status can for Power, Ring Manager, Standby, fault , Relay R1 and R2.
The OID for them are as below.

1. Power Supply P >> oid=".1.3.6.1.4.1.3833.1.1.14.1.1.35.3.1.0"
2. Fault >>  oid=".1.3.6.1.4.1.3833.1.1.14.1.1.35.3.4.0"
3. Ring Manager RM  >> oid=".1.3.6.1.4.1.3833.1.1.14.1.1.35.3.3.0"
4. Standby >> oid=".1.3.6.1.4.1.3833.1.1.14.1.1.35.3.2.0"
5. Relay R1 >> oid=".1.3.6.1.4.1.3833.1.1.14.1.1.35.3.5.0"
5. Relay R2 >> oid=".1.3.6.1.4.1.3833.1.1.14.1.1.35.3.6.0"

Schneider Electric Việt Nam

Phần đính kèm
Port Status and LED Status.xml [2.39 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: