What is the minimum distance required between mounting rails in a NetShelter SX cabinet when installing the AR7725?
Issue:
Customers may want to know what distance is required between the NetShelter SX mounting rails to install the AR7725.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Knowing the minimum distance helps customers understand how much spare room there will be in the cabinet for installing cable management or PDUs.

Resolution:
The AR7725 requires 24.83" (630.68mm) distance between the NetShelter SX mounting rails to mount.

Schneider Electric Việt Nam

Phần đính kèm
AR7725 Duct Kit Spacing.pdf [108.18 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: