How does the underload time delay work on the ATV12 drives?

Issue:
Underload time delay on the ATV12 drives.

Product Line:
Altivar ATV12

Environment:
All

Cause:
Wants to know the underload time delay works.

Resolution:
I/O menu page 53: The Application underload time delay ( ULt) is the time delay before the underload fault occurs. It is adjustable from 0 to 100 secs.
The Application Underload threshold is set to a certain percentage of the FLA of the motor  ( from 20 to 100 of the FLA) that you want the drive to fault.
I_O Input screen shot

:


Schneider Electric Việt Nam

Phần đính kèm
Programming manual.pdf [9.6 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: