How do you set up the ATV61 or ATV71 Drive to check the motor current on the HMI?
Issue:
ATV61/ATV71 Drive to check the motor current on the HMI

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to verify motor current.

Resolution:
Go to the Main menu and then select 1.2 (Monitoring) and then select Motor Current and press Enter.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: