How do you set the line termination resistor on the ATV212 drive set up for Bacnet protocol?
Issue:
Line termination resistor on the ATV212 drive set up for Bacnet protocol.

Product Line:
Altivar ATV212

Environment:
All

Cause:
Needs to terminate his Bacnet line and wants to know how to set the drive up.

Resolution:
Switch SW103 is the line termination resistance switch to put 120 ohms across the data pins A and B.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: