Tìm các câu hỏi thường gặp
PM8000 series meter DNP 3.0 Device Profile Documentation
Issue
A user would like to configure the PM8000 series meter to communicate via the DNP 3.0 protocol and needs the device profile information
Product Line
PM8000 Series Meter
Environment
DNP 3.0 protocol communication with PM8000 series meter
Resolution
The attached PM8000 series meter device profile document explains the implementation of DNP 3.0.
A user would like to configure the PM8000 series meter to communicate via the DNP 3.0 protocol and needs the device profile information
Product Line
PM8000 Series Meter
Environment
DNP 3.0 protocol communication with PM8000 series meter
Resolution
The attached PM8000 series meter device profile document explains the implementation of DNP 3.0.
Đã phát hành cho:Schneider Electric Việt Nam
Phần đính kèm
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: