Is there a way to restore the default username and password for the web page access to the M340 CPU?

Issue
Is there a way to restore the default username and password for the web page access to the M340 CPU?

Product Line
M340

Environment
Windows 10 vesion 1902, BMXP342020 v3.20

Resolution
The user lost the password and cannot access the web pages in the M340 CPU.
They need tp restore the default username and password.

The only way to restore the default username and password is to go into the CPU to delete a specific file.  This requires using an internal proprietary username and password to access it.  Due to security reasons, this username and password cannot be given out to either the customer or a Schneider Electric representative.

In order to restore the default username and password the CPU will need to be sent back for repair.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: