How is the Local/Remote button activated on the Altivar Process keypad?
Issue:
Enabling the Local/Remote button on the Altivar Process keypad

Product Line:
Altivar Process

Environment:
All models

Cause:
The Local/Remote button has no affect to switch between local and remote control.

Resolution:
The factory default setting has this button disabled.  Activate it by going into the Complete Settings menu, Command & Reference menu, and set [HMI CMD] to Stop or Bumpless.

HMI Command

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: