undefined undefined
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
Does the ATV312 require separate 120V control voltage to run the drive?
Issue:
Separate 120V control voltage needed to run an ATV312?

Product Line:
ATV312

Environment:
All

Cause:
Customer does not have 120VAC available

Resolution:
No.  A separate 120Vac is not needed.  Only line voltage is required.
When remote control is used, the VFD provides 24Vdc for the logic inputs.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: