Can you use the VW3A1101 keypad with the ATS48 soft starters?
Issue:
VW3A1101 keypad compatibility with the ATS48 soft starters.

Product Line:
Altistart ATS48

Environment:
All

Cause:
Needs to run a 50ft cable run using the VW3A1101 keypad and cat 5 cable to the ATS48 soft starter.

Resolution:
The VW3A1101 keypad is not compatible with the ATS48 soft starter.   The correct remote keypad part number for the ATS48 is VW3G48101.  The standard cable is 3 meters long.  We do not have any test data to support that you can run this cable with a repeater to get a longer cable run out of it.   You will have to test to see if the remote cable can mounted longer than 3 meters.

Schneider Electric Việt Nam

Phần đính kèm
ATS48_Pinout remote terminal VW3A48101 cable.png [117.19 KB]
ATS48 VW3G48101.pdf [40.52 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: