Where are the S-Flex factory settings listed?
Issue:
S-Flex factory settings listed request

Product Line:
S-Flex

Environment:
All models

Cause:
None

Resolution:
The factory settings for the S-Flex Adjustable Speed Enclosed drive (Class 8839) can be found in Table 18 of the instruction bulletin 30072-451-83 (see below).
https://www.se.com/us/en/download/document/30072-451-83/

Also, the factory settings of the S-flex are stored in a reserved memory location within the drive by the factory during production.  To return the S-flex drive to the default programming, press MODE until AUF is displayed, then scroll down to parameter TYP.  Press ENTER, then up until 8 is displayed on the right hand side of the screen.  Press Enter to reboot the drive and return to the factory default programming for the S-flex system.

IF you are installing a new ATV212 drive in an existing S-Flex enclosure, the parameters will NOT be stored in the drive so you must follow the programming changes listed below.

SFlex parameters

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: