Does Schneider Electric offer the servo motor type BMH1002S0015 ?

No, the BMH1002S0015 is a special version for the company W & H and is a proprietary product which is not available directly from Schneider Electric.
This motor has a special version of winding for the OEM machine and is not replaceable with a standard version.
Customers looking for BMH1002S0015 must contact the OEM machine builder, Windmöller & Hölscher, for a spare motor of this type.

rev 2-19-18

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: