How do you go from 3 wire control to 2 wire control on the ATV312 drives?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Looking to go from 3 wire control to 2 wire control on the ATV312 drives.

Product Line:
Altivar ATV31 and ATV312 drives

Environment:
All

Cause:
The drive was programmed for 3 wire control and now they want change it to 2 wire control.

Resolution:
Programming changes
Go In to the IO menu enter.
find TCC enter
If TCC is 3 C change it to 2C for 2 wire control,
Please note this is a special parameter you will need to hold enter for 3 to 4 seconds.


Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: