NetBotz 200 Temp/Humidity threshold emails do not contain values for temp/humidity
Issue:
Temp/Humidity threshold emails do not contain values for temp/humidity

Product Line:
NetBotz 200

Environment:
NetBotz 200s that are configured to send emails for temperature thresholds.

Cause:
The NetBotz 200 can only alert the title of the alarm within the email.  The title will indicate what the alarm is.  For example, if a high temperature threshold is violated, it will send an email stating that a high temperature threshold has been violated.  The actual temperature value will not be reported via the email.

Resolution:

This is by design. The e-mail will simply state the threshold that was breached as well as the sensor and module for which the threshold was breached. The e-mail will also contain:
Name :
Location :
Contact :
http://IP of NBRK0200

Serial # :
Device Ser #:
Date:
Time:
Code:

Warning - MM: High temperature threshold violation for 'Sensor xxx'

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: