How does Power Monitoring Expert 8.0 installer determine if it has sufficient disk space to install the product?
Issue:
Prior to installing or performing an upgrade, the PME 8.0 Installer checks the system for sufficient disk space, and it will fail if the available disk space doesn't meet the minimum requirements.

Product Line:
Power Monitoring Expert 8.0

Environment:
Power Monitoring Expert Software Upgrade
Power Monitoring Expert Software Installation

Cause:
While running the installer is a definitive way of telling whether there is sufficient free space to run the installer, this information might be useful prior to starting this process.

Resolution:
The attached flowchart provides the logic used by the PME 8.0 Installer to test for disk space.

Schneider Electric Việt Nam

Phần đính kèm
PME8FreeSpaceFlowChart.png [315.68 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: