IEC61850 documentation for VAMP
Issue
Need to program the VAMP relay with the IEC61850 communication.

Product Line
VAMP 5x, 2xx, 3xx

Environment
VAMP set and SCD Editor

Resolution
Attached are the manuals for programming the VAMP for IEC61850

​Latest information is available in m.vamp.fi

Schneider Electric Việt Nam

Phần đính kèm
AN61850.EN002 IEC 61850 interface configuration for VAMP relays.pdf [664.75 KB]
VM61850RELAYSCON.EN002.pdf [777.83 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: