What is the recommended screen resolution for SoMachine V4.1?
Issue
What is the recommended screen resolution for SoMachine V4.1?

Product Line
SoMachine v4.1

Environment
PLC Configuration Software in Windows 7, 8.1, 10

Resolution
The recommended screen resolution for SoMachine v4.1 is 1680 x 1050 pixels at 100% scale.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: