Are we allow to switch the wires associated with the pin out of the harting connector?You can do what you want with the cables which are coming from the "H" version, don't forget to connect the IN0 to the S2_S3 (Feedback loop) ?
Đã phát hành cho:Schneider Electric Việt Nam