On the I/O are they listed as digital. What kind? Encoder? 0-10V? or just on or off.
Inputs are designed to be connected to a potential free contact. Be carefully that there are several types of inputs: - safety inputs, limit switches inputs and alarm inputs. This wiring diagram is depending on the input function.

Schneider Electric Việt Nam