Does the Modicon M580 support the use of Quantum ERIO drops?
Issue
Modicon M580 support for Quantum ERIO drops

Product Line
Modicon M580 PAC, Quantum

Resolution
The Modicon M580 models BMEx584040, 5040 and 6040 will support Quantum ERIO drops when used with Unity 11.0 running Hot Fix 1 or later. Hot Fix 1 will also allow State RAM addressing for the Quantum ERIO drop.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: