What is the replacement for the 8839 58M series enclosed drive?
Issue:
Replacement for the 8839 58M series enclosed drive

Product Line:
8839 58M enclosed custom drives

Environment:
8839 58M enclosed custom only

Cause:
Needs a replacement for the 58M drives

Resolution:
Consider the ATV660 product line as a possible replacement for the old 58M drives.  See attachments to break down the 58M part number and review the ATV660 specifications.  The ATV660 part number can be built in the product selector.  Contact your local distributor for assistance.

Schneider Electric Việt Nam

Phần đính kèm
NHA91297_02 ATV660.pdf [7.26 MB]
8839 58M breakdown.pdf [35.96 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: