How to program the ATV61/71 drive to start/stop using terminals and use the HMI (keypad) as speed control?
Issue:
Wants to program the ATV61/71 drive to start/stop using terminals and use the HMI (keypad) as speed control.

Product Line:
ALTIVAR 61, ALTIVAR 71

Environment:
All

Cause:
N/A

Resolution:
Under drive menu, go to 1.6 [COMMAND] menu:
Set Ref 1 channel to HMI.
Set Profile to separate.
Set Cmd channel 1 to terminals.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: