Why are my Switch Scripts in Vijeo Designer executing at the same time?

Issue:
The execution of the touch scripts setup in a Vijeo Designer Switch are not behaving as expected.

Product Line
Vijeo Designer (all versions)

Resolution:
In Vijeo Designer, when you program a switch to have multiple scripts, they will all execute at once and not sequentially. If you require the first script to be completed before the next one begins, you should either insert a delay long enough for the first script to complete or implement separate switches with separate scripts.

Another alternative is to use Global Actions with "On data change" as the trigger for the script to execute. Once a particular variable has changed data, you could then execute the next sequential script.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: