Are lugs included with ATS22 Soft Starts?
Issue:
ATS22 Soft Starts lugs inclusion

Product Line:
Altistart ATS22

Resolution:
Smaller units (ATS22D17 thru ATS22D88) have a cage style connector to accept power circuit wiring with built-in terminals.
Larger units (ATS22C11 thru ATS22C59) have bus bar landing pads only.  Lugs are not included, but are available for separate purchase. Please see the attached documents for part numbers and instructions.

The ATS22C17S6U can also accept the smaller lug DZ2FG1 (single lug) or DZ1FG6 (set of 6 lugs).

Schneider Electric Việt Nam

Phần đính kèm
ATS22 Power Terminals.pdf [167.22 KB]
ats22_lug_kit_s1a88413_01.pdf [2.38 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: