Cannot change the HTTP or FTP password for the 140NOE77111 using Web Designer.

Issue
Cannot change the HTTP or FTP password for the 140NOE77111 using Web Designer.

Product Line
Quantum Ethernet Module

Environment
140CPU67160, 140NOE77111

Resolution
The selection for HTTP and FTP password on the target security window is greyed out and not selectable.

image1

Due to cyber security reasons, the ability to change the HTTP and FTP passwords for 140NOE77111 Factorycast
module using Web Designer is not allowed.   Changing of the HTTP and FTP passwords for the  140NOE77111
Factorycast module must be performed from the 'Setup' web pages.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: