ION 6200 Meter Replacement Power Supply
Issue
The ION 6200 meter is inoperable (will not start). The power supply unit is not operating correctly and is required to be replaced.

Product Line
PowerLogic ION 6200 meter

Environment
PowerLogic ION 6200 meter power supply unit

Cause
The ION 6200 meter power supply needs to be replaced. The end-user is not required to send the meter back to the factory for an RMA.

Resolution
The power supply unit may be replaced by ordering one of the part numbers below:

P620PB - Standard P240 plug-in power supply (100-240VAC/110-300VDC)
P620PC - P24 plug-in power supply (20-60VDC)

**Note: The 480V power supply option for the ION 6200 meter is no longer available as it is obsolete.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: