Does APC offer a grounding cage nut?
Issue:
Special "grounding" cage nuts can be used to ground an equipment chassis to the cabinet.

Product Line:
NetShelter

Environment:
All versions and serial ranges.

Cause:
Installation instructions may call for grounding cage nuts instead of connecting ground straps to the equipment chassis, then to a busbar.

Resolution:
APC does not currently offer a grounded cage nut.
A better solution is to use AR8395 copper busbar and connect a ground wire from the equipment's chassis ground points directly to the busbar. This makes a much more reliable ground path.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: