What is the range of wavelength acceptable by ACE937 module?
Issue
Specification needed for ACE937 input

Product Line
ACE937

Environment
Sepam 20, 40, 80

Resolution
ACE937 fiber optic interface can accept a minimum wavelength of 792 nm and maximum wavelength of 865 nm. The most common wavelength, as shown in the manual, is 820 nm.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: