Is BMXFCW503 flame retardant
Background:
Customer is using BMXFCW503 on BMXDDI3202K for a project which requires the flame retardant. The datesheet of BMXFCW503 has no such characteristic announced.

Question:
Is BMXFCW503 flame retardant?

Answer:
Yes, it is flame retardant which is listed in cable SPEC(35013778_E06000)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: