How can we get spare parts for removable terminal blocks of TM3 modules?

Article available in these languages: Tiếng Nhật

For TM3 modules using terminal blocks with pitch 5.08 mm, no spare part for the terminal blocks is available.
It concerns the following TM3 module references: TM3DI8x, TM3DQ8x, TM3DM8x, TM3AI2Hx, TM3AQ2x, TM3AQ4x and TM3TM3x.
For those references, a complete TM3 module has to be ordered again in case of connector loss/damaged.

Spare parts references are available for TM3 modules having terminal blocks with pitch 3.81 mm only:
  • TMAT2MSET: including a set of terminal blocks 10 ways and 11 ways with screw terminals
  • TMAT2MSETG: including a set of terminal blocks 10 ways and 11 ways with spring terminals

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: