Is there a conformal coating option for the HMIGTU series?
Yes, the Magelis HMIGTU series are available with conformal coating. Part numbers shown below:

HMIG3UFC Premium Box
HMIG5UFC Open Box

HMIDT351FC 7" Screen
HMIDT542FC 10.4" Screen
HMIDT551FC 10" Screen
HMIDT642FC 12.1" Screen
HMIDT651FC 12" Screen
HMIDT732FC 15" Screen

Schneider Electric Việt Nam