Issue
Need for alternative language packs for APC Network Management Cards installed in a UPS that uses the SUMX or SY application.
Product Line
Network Management cards: AP9630, AP9631, AP9635
Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products
Environment
All serial numbers
Firmware version 6.4, running application SUMX or SY
Resolution
The attached files contain packs for the following languages:
Instructions for updating/changing the language pack can be found in FA156166
Need for alternative language packs for APC Network Management Cards installed in a UPS that uses the SUMX or SY application.
Product Line
Network Management cards: AP9630, AP9631, AP9635
Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products
Environment
All serial numbers
Firmware version 6.4, running application SUMX or SY
Resolution
The attached files contain packs for the following languages:
- French
- Spanish
- Italian
- Japanese
- Russian
- German
- Chinese
- Korean
- Portuguese
Instructions for updating/changing the language pack can be found in FA156166