Is the VW3A3720 Ethernet module for the ATV630 Process drive available?
Issue:
Can I get the VW3A3720 or the Ethernet module for the ATV630 Process drive?

Product Line:
Altivar Process 630

Environment:
All

Cause:
VW3A3720 availability

Resolution:
Yes, it is available and your ATV630 Process drive must be firmware version 1.5 or above to use this option card.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: