Unity Pro V10, Unity Pro crash deploying a Data Structure
Goals and Symptoms:
Opening a structure containing bit rank when this structure is nested in another structure cause a Unity Pro crash.

Example:
Unity Pro setup
Deploying Word_A cause a Unity Pro crash.

Causes and Fixes
It is an error of Unity Pro V10.
It is possible to deploy an instance of such structure instead of the type.
Unity Pro V11 (and higher) is correcting this problem.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: