What is the part number for Combo Ethernet Card on ATV61 and ATV71 drives?
Issue:
What is the part number for Combo Ethernet Card on ATV61 and ATV71 drives?

Product Line:
ATV61, ATV71

Environment:
All

Cause:
N/A

Resolution:
The part number is VW3A3320. It has both the Modbus TCP/IP and Ethernet IP protocols.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: