How do you set the current limit on the ATV61 and ATV71 drives?
Issue:
Setting the current limit on the ATV61 and ATV71 drives

Product Line:
Altviar ATV61 and ATV71 drives

Environment:
All

Cause:
Wants to set up the current limit setting on the drive.

Resolution:
From the Main menu, go into the Drive Menu
Scroll down to the 1.4 motor control menu and press Enter
Select Current Limit, press Enter, and set your current limit value.
The default current limit values will be set to 1.10 X the ATV61 Drives' current ratings and 1.50 X the ATV71 Drives' current rating.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: