How many IFMs can be stacked to an IFE Switchboard Server (LV434011)?
Issue:
End user would like to know how many IFM (Modbus Interface Modules) can be connected to a single IFE (Ethernet Interface) using the Stacking Connector

Product Line
IFE and IFM devices

Environment:
Modbus Communications

Cause:
It is possible to connect multiple IFM's to a single IFE

Resolution:
Twelve (12) IFMs can be stacked to an IFE Switchboard Server (LV434011) via the stacking connector. To find out more information about the stacking connecter please check out FA374688.








Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: