Are there limits to the number of thresholds I can create in StruxureWare DCE?
Issue:

StruxureWare Data Center Expert Threshold Limitations.

Product Line:

InfraStruxure Central
StruxureWare Data Center Expert.

Environment:

Versions 6.2 through 7.x.

Cause:

Creating too many thresholds was seen to cause resource issues and slow the system down.

Resolution:

The following limitations were implemented in InfraStruxure Central and carried over to StruxureWare Data Center Expert.

Enterprise Server can only Create 30,000 Thresholds.
Standard Server can only Create 15,000 Thresholds.
Basic Server can only Create 4,000 Thresholds.

The DCE virtual machine's limits are based on the Enterprise server. Please note that as with license keys, it is suggested that your configuration is limited to the Enterprise, Standard, or basic configurations based on the resources outlined in the virtual machine release notes for your specific version.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: